How offten I should redetermine the 10-parameter for correction of Hard and Soft-Iron effect?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How offten I should redetermine the 10-parameter for correction of Hard and Soft-Iron effect?

跳至解决方案
1,747 次查看
suqianjin
Contributor I

I plan to develop a device that will have a MAG3110 magnetometer installed to measure device's direction. I understand that readings of the magnetometer must be corrected to eliminate Hard and Soft-Iron effect by using 10 parameters, which was determined after a device was completed, using freescale's method to get precise results. My question is should the 10 parameters be re-determined every time of using the device or just need to determine it only once, then store it in the device's memory, and reuse it forever? Thank you very much for your help. 

标签 (1)
0 项奖励
回复
1 解答
1,323 次查看
michaelestanley
NXP Employee
NXP Employee

Generally we recommend that you run magnetic calibration continuously as a background task.  This effectively nulls out variations due to changes in temperature over time.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,324 次查看
michaelestanley
NXP Employee
NXP Employee

Generally we recommend that you run magnetic calibration continuously as a background task.  This effectively nulls out variations due to changes in temperature over time.

0 项奖励
回复