Hi, does Freescale have a multitouch resistive xy sensor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, does Freescale have a multitouch resistive xy sensor?

1,825件の閲覧回数
rupertbg
Contributor I

And if so can it be made into custom shapes/sizes?

Also - would be advantageous to be force-pressure sensitive?

Is there a product like this?

Thanks in advance!

ラベル(3)
0 件の賞賛
返信
1 返信

1,529件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Rupert Bryant-Greene,

Yes, the Freescale CRTOUCH Touch Sensing Platform is a Ready play solution that integrates standard X, Y resistive touch screen detection, pressure detection on 4 and 5 wires, single and double touch detection, gesture detection and 4 capacitive electrodes independent from touch screen.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信