Hi, does Freescale have a multitouch resistive xy sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, does Freescale have a multitouch resistive xy sensor?

1,817 Views
rupertbg
Contributor I

And if so can it be made into custom shapes/sizes?

Also - would be advantageous to be force-pressure sensitive?

Is there a product like this?

Thanks in advance!

0 Kudos
Reply
1 Reply

1,521 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Rupert Bryant-Greene,

Yes, the Freescale CRTOUCH Touch Sensing Platform is a Ready play solution that integrates standard X, Y resistive touch screen detection, pressure detection on 4 and 5 wires, single and double touch detection, gesture detection and 4 capacitive electrodes independent from touch screen.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply