Help with MPR121

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,563件の閲覧回数
Master_col
Contributor III

hallo, my probles is that first i can comunicate with the controller but with other I2C direction that is not on the datasheet. but well that works, what i cant find are the application notes 3893 and 3894 where explain how to configurate the controller. If someone has them or can helpme i wuld be very greatful. thanks for your time and excuse my bad english.

タグ(1)
0 件の賞賛
返信
1 解決策
3,037件の閲覧回数
Joshevelle
Contributor IV

Hello Christian,

Both questions had been answered in the following post:

MPR121 datasheet and app note give wrong i2c slave address (rev 0, 9/2009)

Regards,

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,038件の閲覧回数
Joshevelle
Contributor IV

Hello Christian,

Both questions had been answered in the following post:

MPR121 datasheet and app note give wrong i2c slave address (rev 0, 9/2009)

Regards,

Josh

0 件の賞賛
返信