Generic CSI2 application for S32R45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generic CSI2 application for S32R45

1,714 Views
Mufeeda_P_P
Contributor I

Hi,

We found out that, there is a CSI2 application in RSDK package specifically for TFE82XX. Is there any generic CSI2 application (or standalone CSI2 application)available for S32R45.

 

Regards,

Mufeeda P P

0 Kudos
Reply
3 Replies

1,700 Views
b41937
NXP Employee
NXP Employee

Hello,

 The CSI2 driver is agnostic of the connected frontend. There are 2 applications in RSDK that exemplify in a similar manner how the CSI2 driver can be integrated: RFE Capture and Multi RFE example. Both use the CSI2 driver with TEF82XX frontend. RFE capture may be a better starting point as it only addresses data acquisition. 

Regards,

Tudor

0 Kudos
Reply

1,696 Views
Mufeeda_P_P
Contributor I

Hi,

We checked these 2 applications in RSDK. But we want the standalone CSI2 application for receiving RAW data from the RADAR not for TEF82XX. 

 

Note : If not application, any standalone code to get the frame data in storage device is fine.

 

Regards,

Mufeeda P P

0 Kudos
Reply

1,688 Views
b41937
NXP Employee
NXP Employee

We do not have a standalone CSI2 application as it needs a front-end to connect to. 

If you want to use it with another frontend, you can use the RF_Abstract/RFE driver source code as a reference/example for configuring and using the CSI2 driver for data acquisition.

Best regards,

Tudor

0 Kudos
Reply