Freedom Sensortoolbox Rev. 2.3 not working?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freedom Sensortoolbox Rev. 2.3 not working?

2,291 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi,

has anyone successfully installed and run the new release (Rev. 2.3) of the Freedom Sensor Toolbox?

I worked with an older version (Rev 2.1) before without any issues. Now with the updated release I can not run the "Kinetis Interface Tool" anymore.

I have Win7, 64-bit.

 

Any idea what's going wrong?

 

br

Guenter

42431_42431.PNGCapture.PNG

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-STBC-AGM01&fpsp=1&tab=Design_Too...#

Labels (1)
0 Kudos
Reply
3 Replies

1,624 Views
aswins
NXP Employee
NXP Employee

Hi Guenter,

                 Can you elaborate your problem a little more please?. Is it like you are able to install REV 2.3 but you are getting error when you try to open Kinetis Interface Toolkit? Where in the installation process are you getting the error?

Thanks

Aswin

0 Kudos
Reply

1,624 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi Aswin,

there was no error during the install process. The error appeard when opening the Kinetis Interface Toolkit after installation. But I think the error is gone.

I've updated the software to Rev. 2.3.2 today and it looks like it is working ok now.

I saw in the release notes that the error which I was confronted with has been fixed.

Thanks

Guenter

0 Kudos
Reply

1,624 Views
aswins
NXP Employee
NXP Employee

Hi Guenter,

              Glad that your problem is resolved .

Regards

Aswin

0 Kudos
Reply