Freedom Sensor Toolbox - Firmware download not possible

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freedom Sensor Toolbox - Firmware download not possible

1,096 Views
sam21
Contributor I

Hi there

I'm desperately trying to get the Freedom Sensor Toolbox (CE) (v2.0.0.) running with the FRDM-K64F base and the FRDM-STBC-AGM01 shield.

I did all the updates for DAPLink, but i still get the error message :

"The firmware was not successfully downloaded. Please find the STB-CE User Guide [...]"

When i plug the device in, i see a FRDM-K64FD device and the details.txt contains following information:

# DAPLink Firmware - see https://mbed.com/daplink
Unique ID: 0240000033904e4500293013912700142041000097969900
HIC ID: 97969900
Auto Reset: 0
Automation allowed: 0
Overflow detection: 0
Daplink Mode: Interface
Interface Version: 0244
Bootloader Version: 0244
Git SHA: 5f9092d41cfd6601fef7b3b467fe8f8767b01f84
Local Mods: 1
USB Interfaces: MSD, CDC, HID
Bootloader CRC: 0x251003d3
Interface CRC: 0x0676bc5d
Remount count: 0

Can anyone help me please? I really need to get this stuff going or otherwise the sensor will drop out of the evaluation, which would be pretty sad...

Thank you so much!

0 Kudos
Reply
1 Reply

874 Views
JackITB
NXP Employee
NXP Employee

Hello Matthias,

Which demo GUI would you like to run ?

There are 3 available with your hardware:

pastedImage_1.png

You can try to flash the K64F demo FW manually, simply drag & drop the appropriate binary in the FRDM-K64FD drive.

The binary files are located in the Freedom Sensor Toolbox (CE)\Projects installation folders:

C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\FXAS21002 Gyroscope Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_21002_2.0.bin

C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\FXOS8700 6-axis (Accel, Mag) Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_8700_2.0.bin

C:\Program Files (x86)\NXP\Freedom Sensor Toolbox (CE)\Projects\9 Axis Orientation Sensor Demo\Firmwares\ISSDK\FRDM-K64F_FRDM-STBC-AGM01_Orient_2.0.bin

Then launch the FSTB(CE) and run the associated GUI.

Let me know if this solved your issue.

Regards,   Jacques.

0 Kudos
Reply