Dear Community,
I am using the FXOS8700CQR1 sucessfully on Atmel controller.
But every second time, the calibration fails:
First time I can calibrate it.
xmag average= -474
ymag average=-569
zmag average=-626
when I start the second time, calibration fails with
xmag average= -82
ymag average=-88
zmag average=-374
I have reviewed and compared code with examples here:
FXOS8700CQ - Bare metal example project
Accelerometer and magnetometer FXOS8700CQ example code for MQX4.1.1
Problem I still cannot get it. The problem is reproducible every second time.
I call both calibration from the attached library.
FXO.SetAccelOffset();
and
FXO.CalibrateMagn();
thank you and best regads,
Alain
FXOS8700CQR1 calibration fails every second time,
Dear Alain Fuchs,
It is correct, and can viewed in https://www.nxp.com/docs/en/data-sheet/FXOS8700CQ.pdf .
Best Regards.