FXAS2100X Device Tree Linux Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXAS2100X Device Tree Linux Driver

2,036 Views
bdp42
Contributor IV

Does NXP have a Device-tree compatible linux driver for the FXAS2100X Gyro? There is a Linux driver available but it is not device-tree compatible. Linux kernel is 4.1

Thanks

Bruno

Labels (1)
Tags (2)
0 Kudos
1 Reply

1,716 Views
david_diaz
NXP Employee
NXP Employee

Hello Bruno,

I hope this information still helps you.

Unfortunately, we do not have a Linux driver for the FXAS2100 device.

 

In this case, I can provide you a a .zip file which includes Android 2.3 drivers for MMA845x (MMA8451, MMA8452 or MMA8453), MAG3110, MPL3115 as well as the eCompass driver. The user’s guide is also enclosed on the package. You may use this file as a reference for your design.

 

In case you are interested, please create a new case in order to pass you the material.

 

Regards,

David

0 Kudos