Differential pressure transducer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Differential pressure transducer

1,008件の閲覧回数
Miran
Contributor I

Hi dear,

we have this DPT( MPXV2010DP) we can change range from 0-10kpa to 0-2.5kpa?

0 件の賞賛
返信
3 返答(返信)

986件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Miran,

The pressure measurement range of the MPXV2010DP is fixed at 0 to 10kPa, as it is determined by the design and internal construction of the sensor.

You cannot directly modify it through configuration or calibration.

I would recommend that you consider switching to e.g. the MPXV5004DP with a native range closer to your target. This will provide better resolution and accuracy without the need for additional signal conditioning.

BRs, Tomas

0 件の賞賛
返信

979件の閲覧回数
Miran
Contributor I

Dear Tomas, 

thanks for your response. Our controller installed this part number(MPXV2010DP). It seems that from software changed the range to 2.5kpa.

0 件の賞賛
返信

963件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Miran,

It is likely applying a scaling or interpretation adjustment to the sensor's analog output, rather than actually modifying the sensor's intrinsic measurement range. This is purely a digital adjustment and does not alter the hardware properties of the sensor.

BRs, Tomas

0 件の賞賛
返信