Case pin out for some pressure sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Case pin out for some pressure sensor

ソリューションへジャンプ
2,873件の閲覧回数
jianjunsun
Contributor I

I find some pressure sensor datasheet has no pin-out and pin-out instructions,they are MPXA6115AC6U case 482A-1,MPX5100GP case 867B-4,MPX5010DP case 867C.Please tell me how the pin out and pin instrstuction are they! thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,345件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jianjun,

The pin description is as follows:


1. MPXA6115AC6U (CASE 482A-01, Small Outline Package):

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

SOP.JPG.jpg

2. MPX5100GP (CASE 867B-04, Unibody Package) and MPX5010DP (CASE 867C-05, Unibody Package):

1 – Vout

2 – GND

3 – Vs

4 – N/C

5 – N/C

6 – N/C

Unibody.JPG.jpg

Let me know if you have any other questions.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,345件の閲覧回数
jianjunsun
Contributor I

hi, Tomas.

MPX5010DP is double channel sensor,so the pin out you told me,may be some mistake.

0 件の賞賛
返信
2,345件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jianjun,

You are right that the MPX5010DP is a differential pressure sensor with two input ports, but it is also housed in a Unibody package with the same pinout as the MPX5100GP.

I hope it clarifies your question.


Regards,

Tomas

2,345件の閲覧回数
jianjunsun
Contributor I

OK,Thank you Tomas!

another question,(see the pic below)  the pins V1,V2 is uesed to factory test,we should not conected?

QQ图片20141216202421.jpg  

the pins(see the pic below)  +VOUT,-VOUT is differential output?

QQ图片20141216202445.jpg

0 件の賞賛
返信
2,345件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jianjun,


Yes. V1, V2 and VEX pins are used for factory trimming and then they are laser cut. We recommend to leave those pins floating/unconnected.

As for your second question, please refer to the Different pin styles in pressure sensors documentation.


Regards,

Tomas

0 件の賞賛
返信
2,345件の閲覧回数
jianjunsun
Contributor I

Hi,Tomas,

       Can you tell me the PACKAGE DIMENSIONS of 5010DP and 5100DP ?

the case 867C DIMENSION and package sketch in 5100DP datasheet seems depict two packages,

QQ图片20141223103914.pngQQ图片20141223103938.png

0 件の賞賛
返信
2,345件の閲覧回数
jianjunsun
Contributor I

Tomas,thanks for your wonderful reply!

0 件の賞賛
返信
2,346件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jianjun,

The pin description is as follows:


1. MPXA6115AC6U (CASE 482A-01, Small Outline Package):

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

SOP.JPG.jpg

2. MPX5100GP (CASE 867B-04, Unibody Package) and MPX5010DP (CASE 867C-05, Unibody Package):

1 – Vout

2 – GND

3 – Vs

4 – N/C

5 – N/C

6 – N/C

Unibody.JPG.jpg

Let me know if you have any other questions.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信