Can not found a working ISSDK for FXLS8974CF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can not found a working ISSDK for FXLS8974CF

跳至解决方案
5,511 次查看
shai_b
Senior Contributor II

Dear Team,

My customer has FXLS8974CF EVK but it looks like the ISSDK v1.7 (which is the latest version) is not supporting the FXLS8974CF.

Can you please share with me working ISSDK for FXLS8974CF or working example code that can run on the EVK, your fast responses will be highly appreciated?

Thanks a lot.

Kind Regards,

Shai 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
5,495 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shai,

please find attached a code example for FRDMK22F + FXLS8974. It should also work for the FXLS8974, since they are pin and software compatible.

With Best Regards,

Jozef

在原帖中查看解决方案

6 回复数
5,496 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shai,

please find attached a code example for FRDMK22F + FXLS8974. It should also work for the FXLS8974, since they are pin and software compatible.

With Best Regards,

Jozef

5,480 次查看
shai_b
Senior Contributor II

@JozefKozon, Thank you so much.

KR,

Shai 

0 项奖励
回复
5,489 次查看
Pantos
Contributor II

Dear Jozef,

thank you for your response.

I tried the demo with MCUXpresso and it works properly.

Best regards,

Federico

5,500 次查看
Pantos
Contributor II

Dear Shai,

I am also trying to evaluate the FXLS8974CF with a FDRM-K22F board and I am facing the same problem.

I tried to run the demo of FXLS8962AF, since it should be 100% compatible, but I had no luck both with freeMaster and freedom sensor toolbox.

So I would highly appreciate if ypu could share any solution you found or received.

Kind Regards,

Federico

0 项奖励
回复
4,775 次查看
AmitPurohit
NXP Employee
NXP Employee

Hello Pantos,

Please try with latest FreeMASTER Sensor Tool release available on nxp.com. The latest release support FXLS8974CF along with FXLS8962. I would suggest to use FXLS8974CF eval boards while evaluating the part.

4,723 次查看
shai_b
Senior Contributor II

@AmitPurohit , 

Thanks for letting me know that FreeMASTER Sensor Tool has been updated to support the new family such as FXLS8974CF.

Many Thanks.

KR,

Shai

0 项奖励
回复