Applying Conformal Coating to a circuit card using a MPXV2010GP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Applying Conformal Coating to a circuit card using a MPXV2010GP

跳至解决方案
603 次查看
davebates47
Contributor I

We are about to start production of a circuit card which will use the MPXV2010GP. With the understanding of the vent on the bottom of the part, I am wondering if there are any best practices or advice available on applying conformal coating to the card without gumming up the vent on the bottom? The one solution I can come up with is masking off that area and only installing the part after conformal coating is applied. We would then apply conformal coating to the part's leads with a brush.

Thank you

标签 (1)
0 项奖励
回复
1 解答
584 次查看
RafaR
NXP Employee
NXP Employee

Hi davebates47

Unfortunately, we don't have a document with a specific technique; it generally depends on how the customer wants to use the sensor. Sometimes, people are very creative when it comes to sensor placement.

 

But your idea sounds good, let me recommend just two documents to complement it.

AN1646, Noise Considerations for Integrated Pressure Sensors

AN3150, Soldering Recommendations for Pressure Sensor Devices - Application Notes

You need an account to access to these files

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

在原帖中查看解决方案

0 项奖励
回复
1 回复
585 次查看
RafaR
NXP Employee
NXP Employee

Hi davebates47

Unfortunately, we don't have a document with a specific technique; it generally depends on how the customer wants to use the sensor. Sometimes, people are very creative when it comes to sensor placement.

 

But your idea sounds good, let me recommend just two documents to complement it.

AN1646, Noise Considerations for Integrated Pressure Sensors

AN3150, Soldering Recommendations for Pressure Sensor Devices - Application Notes

You need an account to access to these files

 

I hope this information has helped you, please let me know if you need help with anything else.

Have a great day and best of luck.

0 项奖励
回复