Altimeter MPL311A2 sensor for navigation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Altimeter MPL311A2 sensor for navigation

1,235 次查看
roromiri
Contributor I

Hi everyone,

i would like to know if Altimeter MPL311A2 sensor is applicable in the vehicle for navigation purposes. How sensitive is this sensor to the temperature changes? does it change much? we may change the temperature inside the vehicle by using the air conditioning system or warming inside. do they affect the performance of this sensor?

thank you very much

roro

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

975 次查看
Joshevelle
Senior Contributor I

Hello roro,

tanks for using our community.

The MPL3115A2, has a sensitivity of 0.3m and is temperature compensated from -40°C to 85°C. This is specified in the datasheet Table 2, page 5:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPL3115A2.pdf

Hope it helps.

-Josh

0 项奖励
回复