Accelerometer output data saturation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accelerometer output data saturation

Jump to solution
2,837 Views
koichisakagami
Contributor II

Dear Sirs,
I have one question about MMA8652.

When the acceleration more than a setting range is added to an accelerometer,
how is the output data value ?
Off course, it is under the Absolute maximum ratings.

Is the value saturation (7FF or 800) ?
Or is the value unstable ?

For example.
When the full-scale is set to +- 2g ,
if the accelerometer will be accelerated to 3g,
how is the output data value ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
1 Solution
2,387 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

When acceleration on any axis exceeds the accelerometer’s measurement range (±2g, ±4g or ±8g depending on FS[1:0] bits), the corresponding output is clipped at the full-scale value (0x7FF or 0x800). Considering your example, the 12-bit output value would be 0x7FF.


I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

View solution in original post

0 Kudos
2 Replies
2,388 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Koichi-san,

When acceleration on any axis exceeds the accelerometer’s measurement range (±2g, ±4g or ±8g depending on FS[1:0] bits), the corresponding output is clipped at the full-scale value (0x7FF or 0x800). Considering your example, the 12-bit output value would be 0x7FF.


I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos
2,387 Views
koichisakagami
Contributor II

Dear Tomas san,

Thank you for your answer.

I got it.

Best Regard,

Koichi Sakagami

0 Kudos