Accelerometer motion detection battery drain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accelerometer motion detection battery drain

1,128 Views
rcvutd
Contributor I

Hello,

I am using the MMA8451Q accelerometer in a device and I want to check if that device is being used by someone. So I thought of using the accelerometer's motion detection to read and send an interrupt whenever the device moves. Before I get into the calibration and setting the bytes, I wanted to know if doing this would drain the battery. If this can be done, how long would a 100mAH battery last?

Thank you.

Best Regards.

Labels (1)
0 Kudos
Reply
1 Reply

856 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ramesh,

Table 3 in the MMA8451Q data sheet summarizes the current consumption for different ODRs and operating modes. When using the low power mode and the lowest possible ODR of 1.56Hz, the current consumption is ~6uA, which corresponds to 694 days considering the 100mAH battery. Of course you have to also consider the current consumption of your MCU working ideally in some of the low power sleep modes.  

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply