ADC Calibration Equation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Calibration Equation

3,388件の閲覧回数
xgy_upc
Contributor III

In AN3949 --ADC16 Calibration Procedure and Programmable Delay Block Synchronization, there are two formulae, one for single-terminal input and the other for differential input.

捕获.PNG

Is this formula the gain scaling formula after ADC conversion?  Is Code  the value stored in the result register after gain scaling?Where do the capacitance values Cs and Cn come from?

0 件の賞賛
返信
7 返答(返信)

3,287件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

That's right, the code value is the one that should be stored in the register but as I previously mentioned, you don't need to worry about this calibration since the auto-calibration does this.

Best Regards,
Alexis Andalon

0 件の賞賛
返信

3,287件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello,

Can you let me know which MCU are you using?

Best Regards,

Alexis Andalon

0 件の賞賛
返信

3,287件の閲覧回数
xgy_upc
Contributor III

I'm using KV31F512VLL now

0 件の賞賛
返信

3,287件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello,

The application note that you're pointing to is from an old MCU, for this MCU the module already has a function for calibration. If you check in the reference manual the chapter 32.4.5 Calibration function, you could check the details of this feature.

Best Regards,

Alexis Andalon

0 件の賞賛
返信

3,287件の閲覧回数
xgy_upc
Contributor III

Dear Alexis Andalon,

 

I have read the KV31 reference manual about the calibration function.I think the old MCU in the application notes is basically the same as the ADC calibration of KV31.I just want to know what those two formulas mean in detail

Best Regards,

0 件の賞賛
返信

3,287件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello 相国 尹,

The nominal capacitance will be the ideal capacitance need it to match the sample and the sampled one will be the input capacitance that you can check in the datasheet.

The gain value will be as the next figure show, the multiplication value after the conversion to match the ideal sample.

pastedImage_1.png

Best Regards,

Alexis Andalon

0 件の賞賛
返信

3,287件の閲覧回数
xgy_upc
Contributor III

So,Is this formula the gain scaling formula after ADC conversion?  Is Code  the value stored in the result register after gain scaling?

0 件の賞賛
返信