writing PCR using ssscli

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

writing PCR using ssscli

1,582件の閲覧回数
Henrik78
Contributor I

Hello everyone,

I just set up a test using an RPI3 and the SE050ARD-E evaluation board. I did some first tests using the ssscli tool and till now I managed to get some examples working, but what I can't figure out is how to create a PCR object and write and read to or from it.

I can run the "se05x_PCR" example, but I don't know how to do it using the ssscli tool?! Is this possible at all?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,565件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Henrik78 ,

 

The ssscli doesn't support PCR, and this tool is recommended for develop purpose, but for production, you have to write application code based on the MW something like se05x_PCR.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信