programmable/ erasable ICODE DNA/slix

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

programmable/ erasable ICODE DNA/slix

2,937 次查看
vamsikrishna_ta
Contributor II

 

are there any kind of IC/Tags/Boards or simulators which acts as icode Dna(must support ISO 15693) and responds to all commands, what the exact intension is

1) i want to change its uid.

2). i want to erase and rewrite all the blocks even they are locked / read or write protected.

3. a kind of factory reset where it the keys can be reconfigured even they are locked and activate.

 

标记 (4)
0 项奖励
回复
3 回复数

2,929 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vamsikrishna_ta ,

 

Actually I have no idea of such kind product/IC, but what is the purpose you are looking for this kind of product? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,916 次查看
vamsikrishna_ta
Contributor II

hi @Kan_Li ,

we need to use a lot of icode dna tags for testing purposes, in the process we are wasting many tags as once the tag is programmed with key and activated we cannot able to modify the contents on it . so ,our plan is to reduce programming effors and wastage of tags, we are searching out for a solution that acts a icode dna tag that can be erasable although it is locked and protected.

0 项奖励
回复

2,902 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vamsikrishna_ta ,

 

Thanks for the clarification! Actually UID is permanently set by NXP and is locked(read only), so it is not possible to change it out of factory.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复