porting SE050 driver to U-Boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

porting SE050 driver to U-Boot

ソリューションへジャンプ
4,185件の閲覧回数
a_1359
Contributor II

Hello community,
 
We are planning to use SE050 in our design to do signature verification of the Linux kernel at U-Boot stage as part of the secure boot process.

Is there any official port of SE050 driver to U-Boot? mainline and/or vendor U-Boot?
If yes, where can I find it?
If not, what would be the process to port it? are there some guidelines specifically for porting to U-Boot?

Thanks for your support!
Best regards,

A_1359

0 件の賞賛
返信
1 解決策
4,173件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @a_1359 ,

 

For U-Boot, we have no SE05x integration, but we provide an app note for that topic. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12448.pdf for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,174件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @a_1359 ,

 

For U-Boot, we have no SE05x integration, but we provide an app note for that topic. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12448.pdf for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信