how to set RSA private key into SE050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to set RSA private key into SE050

7,992 Views
yang_lee
Contributor III

Hi everone, now I want to set RSA private key into SE050 but this function return fail: sss_key_store_set_key(). Is there a problem with the way I pass parameters to that function? Please help me.

My code below:

sss_status_t ex_sss_entry_user_set_privKey(ex_sss_boot_ctx_t *pCtx, uint32_t objectID, uint8_t *key_inject, size_t keyLen,)
{
  sss_status_t status = kStatus_SSS_Success;
    /* Policies for key */
    const sss_policy_u key_withPol = {
        .type = KPolicy_Asym_Key,
        /*Authentication object based on SE05X_AUTH*/
        .auth_obj_id = objectID,
        .policy = {
            /*Asymmetric key policy*/
            .asymmkey = {
                /*Policy for sign*/
                .can_Sign = 1,
                /*Policy for verify*/
                .can_Verify = 1,
                /*Policy for encrypt*/
                .can_Encrypt = 1,
                /*Policy for decrypt*/
                .can_Decrypt = 1,
                /*Policy for Key Derivation*/
                .can_KD = 1,
                /*Policy for wrapped object*/
                .can_Wrap = 1,
                /*Policy to re-write object*/
                .can_Write = 1,
                /*Policy for reading object*/
                .can_Read = 1,
                /*Policy to use object for attestation*/
                .can_Attest = 1,
            }
        }
    };
 
    /* Common rules */
    const sss_policy_u common = {
        .type = KPolicy_Common,
        /*Authentication object based on SE05X_AUTH*/
        .auth_obj_id = objectID,
        .policy = {
        .common = {
        /*Secure Messaging*/
        .req_Sm = 0,
        /*Policy to Delete object*/
        .can_Delete = 1,
        /*Forbid all operations on object*/
        .forbid_All = 0,
    }
    }
    };
 
    /* create policy set */
    sss_policy_t policy_for_ec_key = {
        .nPolicies = 2,
        .policies = { &key_withPol, &common }
    };
#ifdef GET_FREE_MEM
  sss_se05x_session_t *pSession = (sss_se05x_session_t *)&pCtx->session;
  uint16_t free_mem = 0;
#endif
 
  /* initialize keyObject with key store */
  status = sss_key_object_init(&key_object, &pCtx->ks);
  if (status != kStatus_SSS_Success)
  {
    return status;  /* return error if can't initialize keyObject */
  }
 
/* allocate/pre-provision memory for new key */
  status = sss_key_object_allocate_handle(&key_object,
                                          objectID,
                                          kSSS_KeyPart_Private,
                                          kSSS_CipherType_RSA_CRT,     
                                          keyLen,
                                          kKeyObject_Mode_Persistent);
  if (status != kStatus_SSS_Success)
  {
    return status;
  }
 
/* moves data[] from memory to the destination key store */
  status = sss_key_store_set_key(&pCtx->ks, &key_object, key_inject, keyLen, keyLen * 8, &policy_for_ec_key, 0);
  if (status != kStatus_SSS_Success)
  {
    return status;
  }
 
  return status;   /* return successful if save data successfully */
}
Labels (1)
Tags (1)
0 Kudos
Reply
11 Replies

7,962 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

Which SE05x variant are you playing with? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,953 Views
yang_lee
Contributor III

Hi Kan, 

Thanks for reply, I am using SE050C2HQ1 for my product. It seems to support RSA.

yang_lee_0-1761720445844.png

 

In addition, when I use OM-SE051 ARD-E Dev Kit to run seTool to set RSA key (using PlugAndTrust_v04.07.00_20250210), I get an error described as below image:

yang_lee_1-1761720788886.png

 

Thanks,

 

 

0 Kudos
Reply

7,902 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

Please try with RSA RAW instead, the RSA CTR doesn't accept the pri key value, please check the APDU spec for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,868 Views
yang_lee
Contributor III

Hi @Kan_Li ,

I noticed that the code in seTool is using kSSS_CipherType_RSA_CRT.

yang_lee_0-1761913504498.png

 

And I also tried with raw data but still failed. The RSA key that I pass into the ex_sss_entry_user_set_privKey function is attached below:

Is there any problem with this raw key?

Thanks

0 Kudos
Reply

7,792 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

How did you generate the RSA Key for SeTool externally?  Actually we have a demo of se05x_Delete_and_test_provision which provides an example for that purpose, please kindly refer to the following for details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,787 Views
yang_lee
Contributor III

Hi @Kan_Li,

I generated the RSA key by Openssl.

I think I will use it with ECC key instead of RSA key because now I have successfully used it with ECC key. Thanks for your kind support.

Brg.

0 Kudos
Reply

7,776 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

Thanks for the clarification! 

 

Please kindly have SeTool examples regarding RSA key pair as below:

openssl genpkey -algorithm RSA -out RsaKeyPair2048.pem -pkeyopt rsa_keygen_bits:2048
./seTool setRsaKeyPair 2048 0xF0000211 RsaKeyPair2048.pem none

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,746 Views
yang_lee
Contributor III

Hi @Kan_Li,

Thanks for suggestions.

I built Plug & Trust MW version 04.07.00 and tried with SE051 but it still fails when using RSA key while succeeds with ECC key. Details are shown in the image below:

yang_lee_1-1762248358170.png

 

Brg.

Tags (1)
0 Kudos
Reply

7,705 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

Was the RSA key file generated with the following command?

openssl genpkey -algorithm RSA -out RsaKeyPair2048.pem -pkeyopt rsa_keygen_bits:2048

Are you using OM-SE050E-ARD ? Indeed SE050E doesn't support RSA.

 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,664 Views
yang_lee
Contributor III

Hi @Kan_Li,

1. “Was the RSA key file generated with the following command?”
Yes, the RSA key file was generated using the command:
"openssl genpkey -algorithm RSA -out RsaKeyPair2048.pem -pkeyopt rsa_keygen_bits:2048."

2. “Are you using OM-SE050E-ARD? Indeed SE050E doesn't support RSA.”
No, I am using OM-SE051-ARD (SE051C2HQ1) instead of OM-SE050E-ARD. Actually I have both of these development kits and both build SE-PLUG-TRUST-MW_04.07.00 to run the examples with SE05x. Besides, the product I am developing is using SE050C2HQ1 (for both Android and Bare metal platform), everything seems to work fine except RSA.

Best regard.

 

 

0 Kudos
Reply

7,507 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @yang_lee ,

 

Sorry, my bad! Seems this tool has updated its parameters, please use the following command instead.

seTool setRSA 2048 0xF0000211 RsaKeyPair2048.pem none

Please kindly have my result as below:

Kan_Li_0-1762482313155.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply