evaluate A71CH chip on arm9,linux platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

evaluate A71CH chip on arm9,linux platform

2,322件の閲覧回数
ratheendran_r
Contributor I

Hi,

We want to evaluate A71CH chip for our  IOT device,this developed on arm9 linux system.

doc : A71CH Quick start guide for OM3710A71CHARD and i.MX6UltraLite

I  refereed the above document, it discusses on prebuild images,there are no pointers on where  to get  source and sdk. Ideally would like to try this on any of the open-source platform like raspberrypi,beaglebone. let me know if any one has made previous such attempts and would like to share here.

Thanks,

Ratheendran

ラベル(1)
0 件の賞賛
返信
1 返信

2,144件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

The SDK it's available under the Software and Tools tab of the device : 

A71CH | Plug and Trust for IoT|NXP  

I believe the one you are looking for will be the i.MX A71CH Host Software package which targets the IMX6UL-EVK board. Part of the software is compatible with gcc on Linux or Cygwin.

Regards, 

0 件の賞賛
返信