Update binary object with policy fails.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Update binary object with policy fails.

1,706 次查看
deang
Contributor III

I can create, read, and delete a binary object created with the following policies (below).  However updating the file with Se05x_API_WriteBinary()   function fails.  However, if I create a binary object without any policies I can update it with Se05x_API_WriteBinary() .   Is this the expected behavior with polices?   

Dean G.

 

static sss_policy_u file_withPol = {

                .type = KPolicy_File,

                /*Authentication object based on SE05X_AUTH*/

                .auth_obj_id = 0, // AES authentication

                .policy = {

                                /* binary file policy*/

                                .file = {

                                                                /** Allow to write the object */

                                                                .can_Write = 1,

                                                                /** Allow to read the object */

                                                   .can_Read = 1

                                }

                }

};

 

/* Common rules */

static sss_policy_u file_common = {

                                .type = KPolicy_Common,

                                /*Authentication object based on SE05X_AUTH*/

                                .auth_obj_id = 0,  // AES authentication

                                .policy = {

                                                .common = {

                                                /*Secure Messaging*/

                                                .req_Sm = 0,

                                                /*Policy to Delete object*/

                                                .can_Delete = 0,

                                                /*Forbid all operations on object*/

                                                .forbid_All = 0,

                                }

                }

};

0 项奖励
回复
1 回复

1,701 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

How about setting   .can_Delete = 1? 

 

Please kindly let me know if the problem is still there.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复