Unusual error code 0x6D00

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unusual error code 0x6D00

Jump to solution
2,921 Views
deang
Contributor III

Getting an unusual error code when I try the `Se05x_API_CheckObjectExists()` api. The result buffer contains error code 0x6D00.  Any idea what this means?

I'm using the nano-package.

Unencrypted connection.

Thanks,

Dean

 

0 Kudos
Reply
1 Solution
2,879 Views
deang
Contributor III

I figured out the problem.  Another part of the code was closing the session before the call to Se05x_API_CheckObjectExists().

 

 

View solution in original post

0 Kudos
Reply
2 Replies
2,880 Views
deang
Contributor III

I figured out the problem.  Another part of the code was closing the session before the call to Se05x_API_CheckObjectExists().

 

 

0 Kudos
Reply
2,907 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

This code means the instruction is not supported/invalid. Would you please tell me which example and variant of se05x are used in your test? Is it possible to share some code snippet if you are testing your own application code? It would be great helpful if you can share the full log for analyzation.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply