Stateless key management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stateless key management

Jump to solution
1,659 Views
psvz
Contributor IV

Hi Kan,

Re SE050 APDU Specification (nxp.com)

4.7.2 ImportExternalObject

Note: The APDU “ImportExternalObject” must not be used without first contacting
NXP to avoid potential problems. If you have used or plan to use the APDU
“ImportExternalObject,” please make sure you contact your NXP representative.

I consider this as an alternative to KEK, perhaps unnecessary complicated. Could you point me out to any source code exemplifying this workflow? Why does it say to contact NXP representative? 

Labels (1)
0 Kudos
Reply
1 Solution
1,628 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Please kindly refer to "simw-top/doc/demos/se05x/se05x_ImportExternalObjectPrepare/Readme.html" for details. There are some guide for the cases using this command , depending on the purpose you want to achieve, so if you want to use this command, please kindly tell us what you want to do and we will check if there is anything you have to take care.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,629 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Please kindly refer to "simw-top/doc/demos/se05x/se05x_ImportExternalObjectPrepare/Readme.html" for details. There are some guide for the cases using this command , depending on the purpose you want to achieve, so if you want to use this command, please kindly tell us what you want to do and we will check if there is anything you have to take care.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply