Session-less access with SE050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Session-less access with SE050

跳至解决方案
3,013 次查看
ninomedj
Contributor I

Hi, i'm intrested to know more about session-less acess, for example if we take the se05x_Minimal.c example we call Se05x_API_GetFreeMemory function that construct an apdu and send it to the SE and receive the free memory availeble, my qst is can we excute this fct or any SE050 layer fct with session-less acess and how can we do it? 

Thank you.

0 项奖励
回复
1 解答
3,007 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ninomedj ,

 

Yes, it is possible, you just need to make sure no Auth option is enabled before you run any SE05x demo.

Kan_Li_0-1649744932862.png

BYW, which platform are you testing with SE050?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,008 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ninomedj ,

 

Yes, it is possible, you just need to make sure no Auth option is enabled before you run any SE05x demo.

Kan_Li_0-1649744932862.png

BYW, which platform are you testing with SE050?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,005 次查看
ninomedj
Contributor I

Hi @Kan_Li ,

Thank you for your answer , i'm currently working on an Atmel sam4sd32c.

Have a great day.

0 项奖励
回复