SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE05x-PLUG-TRUST-MW version 04.05.00 is missing PSA.proto

1,943 Views
stefanct
Contributor IV

nxp_iot_agent/doc/protobuf/Dispatcher.proto is importing PSA.proto which is not contained in the archive.

0 Kudos
Reply
4 Replies

1,903 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @stefanct ,

 

The PSA.proto file is used just in case of RW61x target which is not yet supported in P&T MW release; for this reason the PSA.proto file is excluded.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

1,886 Views
stefanct
Contributor IV
It breaks execution of 'semslite_json_converter.py . protoc'. If it's not included it should not be referenced in Dispatcher.proto
0 Kudos
Reply

1,881 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @stefanct ,

 

Have you tried to comment the reference out in Dispatcher.proto? Does it work for your case?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,875 Views
stefanct
Contributor IV

Yes, of course. The PSA definitions are used in two places that have to be disabled as well, see attachment.