SE050F2 - EMVco compliance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050F2 - EMVco compliance

ソリューションへジャンプ
4,818件の閲覧回数
hitesh_gambhava
Contributor I

Hi,

I am exploring having FIPS and EMVco compliance in a single chip. I found SE050F2 has FIPS compliance and NFC interface as per ISO 1443. So curious to know how difficult to get the approval of EMVco on SE050F2?

 

Thanks,

Hitesh

0 件の賞賛
返信
1 解決策
4,772件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

The SE05x platform is not EMVCo certified and it would be quite some effort . Also the banking applets are so far not qualified on this platform. There is no plan to certify SE050/51 with EMVCo. If no I2C is needed then P71 JCOP4 could be a solution, this platform is EMVCo and FIPS certified. There only the platform is certified, so still an applet which implements the use case needs to be uploaded and then the whole package be FIPS-certified. 

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,773件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

The SE05x platform is not EMVCo certified and it would be quite some effort . Also the banking applets are so far not qualified on this platform. There is no plan to certify SE050/51 with EMVCo. If no I2C is needed then P71 JCOP4 could be a solution, this platform is EMVCo and FIPS certified. There only the platform is certified, so still an applet which implements the use case needs to be uploaded and then the whole package be FIPS-certified. 

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,767件の閲覧回数
hitesh_gambhava
Contributor I

Hi Ken,

This information is really helpful. Thanks!

Can the SMARTMx3 platform have the capability to use a host controller as well to connect some sensors on SPI and UART?

--

Best Regards,

Hitesh

0 件の賞賛
返信
4,745件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

The SmartMX3 is just a host controller, do you mean to connect it with some sensors via SPI/UART? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,672件の閲覧回数
hitesh_gambhava
Contributor I

Hi Kan,

I was under the impression that P71 JCOP4 is part of the SmartMX3 controller series. How can I get further information about P71 JCOP4, like its size/package and interface to communicate with a host controller, etc.?

Also, are there any charges/fees for the crypto library for EMVco or FIPS use cases?

Thanks,

Hitesh

0 件の賞賛
返信
4,646件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hitesh_gambhava ,

 

The documents for P71 JCOP4 are under NDA, if you have not signed it with NXP yet , you may request it online, and then request them from the Secure File according to the following link:

https://www.nxp.com.cn/docs/en/user-guide/nxp-secure-access-rights-registration.pdf

Kan_Li_0-1687837046363.pngKan_Li_0-1687837046363.png

 

and for commercial topic, please kindly contact your local NXP sales representatives. 

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
4,608件の閲覧回数
hitesh_gambhava
Contributor I

Hi Kan,

We have signed NDA with the NXP team. Thank you for the information.

 

Thanks,

Hitesh

0 件の賞賛
返信