SE050C2HQ1/Z01SDZ- Termination finish

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SE050C2HQ1/Z01SDZ- Termination finish

跳至解决方案
2,316 次查看
shai_b
Senior Contributor II

Hello team,

We need your advice regarding the termination finish of #SE050C2HQ1/Z01SFZ.

  a. In the case of 100% tin please advise:
      i. What kind of tin is used, matte or bright?
      ii. Do you run annealing (1h baking in 150°c max 24h past plating)?
      iii. Do you make tin whiskers test according to JSDEC22-A121 or JEDEC201?
      iv. What is the minimum thickness of the leads coating finish layer?
      v. What is the intermediate layer material?
b. In the case of 100% Gold Plating:
      i. What is the material used under the gold finish?
      ii. What is the minimum Gold coating thickness?
c. In case of other coatings than those above, please mention it.

Please advise back, thanks in advance.

Kind regards,

Shai

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,201 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Shai,

The termination finish of HX2QFN20 is PPF plating (Pre-Plated Leadframe).

The plating composition is specified in the LF drawing as detail below.

pastedImage_1.png

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,201 次查看
shai_b
Senior Contributor II

Hello team,

There is any update?

kind regards,

Shai

0 项奖励
回复
2,202 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Shai,

The termination finish of HX2QFN20 is PPF plating (Pre-Plated Leadframe).

The plating composition is specified in the LF drawing as detail below.

pastedImage_1.png

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------