SE050: writing cardlets/applets via GlobalPlatform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050: writing cardlets/applets via GlobalPlatform?

3,932 Views
JWilkes
Contributor I

Hello NXP support, hello everybody!

The SE050 specifications and data sheets list this family as having JavaCard version 3.0.5 and
GlobalPlatform GP 2.3.1.

The variant identifier lists which Applets are pre-installed. And there's 50k User memory.

However, I didn't find any documentation on whether and how custom cardlets/Applets can be installed.

Q 1: Is it possible at all to install cardlets on SE050?

Q 2: If possible, which SE050 variants are suitable, and which document IDs (including Docstore) are relevant for this?

 

Thank you for your help,

Jo Wilkes

Labels (1)
0 Kudos
Reply
3 Replies

3,923 Views
JWilkes
Contributor I

Do all SE051 variants support custom applets?

0 Kudos
Reply

3,915 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @JWilkes ,

 

To upload custom applets , you have to select P2 variant, others just support IoT applets update as well as Configure EdgeLock SE051 using the PERSO applet. Please kindly refer to https://www.nxp.com/webapp/Download?colCode=AN13015 for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,928 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @JWilkes ,

 

I am sorry, but SE050 doesn't support custom applet, you have to look at SE051 instead. Please kindly refer to https://www.nxp.com/products/security-and-authentication/authentication/edgelock-se051-proven-easy-t... for details.

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------