SE050 and Middleware v4.3.0 - Possible bug with Openssl engine?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 and Middleware v4.3.0 - Possible bug with Openssl engine?

1,237件の閲覧回数
TonyMo
Contributor I

I'm using the SE050F2 With middleware v4.3.0. I'm using the an openssl engine so external libs like security-xml-c can leverage the RSA keys in the SE050.

I'm finding a failure in sss/plugin/openssl/engine/src/ax_sssEngine_rsa.c in the function EmbSe_RSA_Priv_Encrypt() where if the RSA padding selected is not set to RSA_NO_PADDING, the call fails. Is this correct or a bug? xml-security-c uses RSA padding RSA_PKCS1_PADDING which complies with the XML security standard. 

TonyMo_0-1689338999815.png

 

Also, in the same function EmbSe_RSA_Priv_Encrypt(), I notice that sss_asymmetric_context_init() uses the kMode_SSS_Decrypt and makes a call to sss_assymmetric_decrypt(). I intuitively would expect that RSA_Priv_Encrypt() is doing "encrypt" operations, not "decrypt" operations. Is this a bug?

TonyMo_1-1689339252997.png

 

Thank you for your help.

Cheers,

Tony

 

0 件の賞賛
返信
2 返答(返信)

1,178件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @TonyMo ,

 

Indeed the function EmbSE_RSA_Priv_Encrypt is actually the method referenced to “sign” data. With RSA the signature is correctly created with the method “decrypt”. From the openSSL documentation:

Kan_Li_0-1689903033667.png

I agree that the engine’s function name is misleading as it actually should be the signing function.

 

For the RSA padding methods support, we are checking with the R&D now, will let you know when I have any more info from there.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信

1,155件の閲覧回数
TonyMo
Contributor I

Thank you Kan. There is no concern with the SE050 not being to support RSA padding. I was able to leverage Openssl's RSA padding commands to achieve what I needed.

 

0 件の賞賛
返信