SE050 RSA OAEP mode support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 RSA OAEP mode support

ソリューションへジャンプ
3,131件の閲覧回数
bboozzoo
Contributor I

Hi,

I'm trying to encrypt small pieces of data using RSA2048 key stored inside SE050. The SE050 is being access through MW v04.03.00. The requirement was to use RSA-OAEP mode with SHA256 digest. However, from experimentation, I only seem to be able to successfully encrypt anything by passing `kAlgorithm_SSS_RSAES_PKCS1_OAEP_SHA1`. Attempting to use any other digest results in 1010565120 (0x3c3c0000) status error. Can you confirm if this is a limitation of SE050?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,085件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, so far only SHA1 is supported for digest. Please kindly refer to the following for details.

Kan_Li_0-1691983939869.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,086件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bboozzoo ,

 

Yes, so far only SHA1 is supported for digest. Please kindly refer to the following for details.

Kan_Li_0-1691983939869.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
3,020件の閲覧回数
bboozzoo
Contributor I
Thanks!
0 件の賞賛
返信