SE050 Docs for Java

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 Docs for Java

1,865 Views
julian_sauer
Contributor III

Are there any Docs using the Middleware via Java? In the Webinar they often mention a Android Development with the SE050

Labels (1)
0 Kudos
Reply
1 Reply

1,760 Views
Kan_Li
NXP TechSupport
NXP TechSupport

I am sorry, but so far no such kind of build option for the Middleware.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------