SCP03 key version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCP03 key version

Jump to solution
3,038 Views
deang
Contributor III

Is there any information on how to set/use the key version when rotating SCP03 keys and using them?  In nxScp03_CP_InitializedUpdate() (in se05x_APDU_impl.c) the key version is set here:

     tlvHeader_t hdr = {{CLA_GP_7816, INS_GP_INITIALIZE_UPDATE, keyVersion, 0x00}};

For SCP03 the version is 0xB.  If I rotate the SCP03 keys should this number change?

I'm using the NXP Nano package.

Dean

0 Kudos
Reply
1 Solution
3,010 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

The key version number (KVN) is the identifier of the slot where the key is stored. It shall stay the same, the existing key should get exchanged on the key rotation to overwrite the previously stored default key. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,011 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

The key version number (KVN) is the identifier of the slot where the key is stored. It shall stay the same, the existing key should get exchanged on the key rotation to overwrite the previously stored default key. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,970 Views
deang
Contributor III

Thanks @Kan_Li 

Dean

0 Kudos
Reply