SCP03 default keys

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,460件の閲覧回数
deang
Contributor III

The default SCP03 keys listed in: https://www.nxp.com/docs/en/application-note/AN12436.pdf  are incorrect.  The following is a code snippet from the PlugTrust library (ex_sss_tp_scp03_keys.h):

// Variant ==> OEF ID
// SE050A1 ==> A204
// SE050A2 ==> A205
// SE050B1 ==> A202
// SE050B2 ==> A203
// SE050C1 ==> A200
// SE050C2 ==> A201
// Development Board ==> A1F4 (DEVKIT)

//SE051C ==>0xA8FA
//SE051A ==>0xA920
//SE050E ==>0xA921
//SE051W(Fira) ==>0xA739
//A5000 gen ==>0xA736
//SE050F2 ==>0xA92A

Are these mappings correct?

Also when will the AN12436 app note be updated?

Dean

 

0 件の賞賛
返信
1 解決策
3,417件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Yes, there is some OEF ID info issue in table 6, please refer to table 2 instead, alternatively you may refer to the mapping info you found in the PlugTrust library (ex_sss_tp_scp03_keys.h). The update for AN12436 is in progress, I will let you know when it is available.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,417件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Yes, there is some OEF ID info issue in table 6, please refer to table 2 instead, alternatively you may refer to the mapping info you found in the PlugTrust library (ex_sss_tp_scp03_keys.h). The update for AN12436 is in progress, I will let you know when it is available.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,405件の閲覧回数
deang
Contributor III

Thanks Kan.

I double checked and I've got all of the variants and correct keys set in my code. For ease of refence, here's the list of OEFIDs and variants.

A201 == SE050C2
A200 == SE050C1
A921 == SE050E2
A92A == SE050F2
A204 == SE050A1
A205 == SE050A2
A43B == SE050D2
A202 == SE050B1
A203 == SE050B2
A77E == SE050F2

Dean

0 件の賞賛
返信