Request: Implement C_UnwrapKey in SIMW Top PKCS#11 (SE05X) for CMS ECDH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Request: Implement C_UnwrapKey in SIMW Top PKCS#11 (SE05X) for CMS ECDH

1,184 Views
vishwaec08
Contributor I

Hello NXP Team,

We need C_UnwrapKey (AES-CBC/AES-CBC-PAD) implemented in SE05X SDK PKCS#11 to enable CMS ECDH handle-only decrypt on SE05X.

Currently C_UnwrapKey returns CKR_FUNCTION_NOT_SUPPORTED in sss_pkcs11_pal_core.c. The flow requires unwrapping the CMS CEK on-token using the derived AES handle plus the 16-byte IV from CMS.

 

Regards
Vishwa

0 Kudos
Reply
2 Replies

1,148 Views
vishwaec08
Contributor I

Hi,

The overall idea is that we want to encrypt and decrypt the data using OpenSSL CMS with an EC key.

For reference, the OpenSSL commands are listed below.

pkcs11-tool --module /usr/lib/libsss_pkcs11.so --slot 1 --keypairgen --key-type EC:prime256v1 --label "sss:20202022"

OPENSSL_CONF=engine.conf openssl req -engine pkcs11 -new -key "pkcs11:object=sss:20202022;type=private" -keyform engine -out ec_req.pem -x509 -subj "/CN=Test EC" -days 365

OPENSSL_CONF=engine.conf openssl x509 -engine pkcs11 -signkey "pkcs11:object=sss:20202022;type=private" -keyform engine -in ec_req.pem -out ec_cert.pem

openssl cms -encrypt -binary -outform DER -aes128 -in smcont.txt -recip ec_cert.pem -out test_ec.cms

OPENSSL_CONF=engine.conf openssl cms -decrypt -binary -inform DER -engine pkcs11 -keyform engine -inkey "pkcs11:object=sss:20202022;type=private" -recip ec_cert.pem -in test_ec.cms -out smtst.txt

 

0 Kudos
Reply

1,162 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vishwaec08 ,

 

I have forwarded your feature request to the expert team, and will let you know when I have any feedback from there.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply