Reading RESERVED_ID_UNIQUE_ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading RESERVED_ID_UNIQUE_ID

ソリューションへジャンプ
2,310件の閲覧回数
deang
Contributor III

1. Are there any special requirements for reading the unique ID?  Specifically the RESERVED_ID_UNIQUE_ID?  I am connected using a plain connection, the error I keep running into is SM_ERR_CONDITIONS_OF_USE_NOT_SATISFIED.  Do I need to be connect via SCP03?

2. What is the size of this data?

Thanks,

Dean

0 件の賞賛
返信
1 解決策
2,273件の閲覧回数
deang
Contributor III

Hi Kan,

Thanks for the help.  Using the exact size (18 bytes) fixed the problem. I do think the Se05x_API_ReadObject() should allow for a larger than necessary buffer vs. the exact size.  

Dean

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,288件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

No specific requirement to read this object, we provide a code snippet in nxp_iot_agent_demo for that purpose, please kindly refer to the following for more details.

Kan_Li_0-1690947142749.png

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
2,274件の閲覧回数
deang
Contributor III

Hi Kan,

Thanks for the help.  Using the exact size (18 bytes) fixed the problem. I do think the Se05x_API_ReadObject() should allow for a larger than necessary buffer vs. the exact size.  

Dean

0 件の賞賛
返信