Question, A1006 and A71CH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, A1006 and A71CH

2,257 Views
SLICE
Contributor IV

Dear team,

I found the following description in A1006 datasheet.

"The A1006 secure authentication IC extends this portfolio for applications requiring tamper-resistant, secure, one-way authentication."

On the other hand, A71CH is said to support two-way authentication.

Could you show me why A1006 can support one-way auth while A71CH supports two-way auth?

Thanks,

Miyamoto

0 Kudos
Reply
1 Reply

1,989 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Miyamoto,

The one-way authentication means the A1006 proves it is authentic to anybody, the A1006 cannot check who is challenging it. The Hosts sends a challenge the A1006 answers through the knowledge of the asymmetric secret with a answer which the host can check with the public part of the asymmetric secret.

 

The A71CH when forming an encrypting channel is doing the authentication in both directions using symmetric cryptography. In that form the host first proves that it knows the secret key to the A71CH and then the A71CH answers with a prove that it also knows the secret key. This means both parties can be sure that the other side has knowledge of the secret.

 

The A71CH also can do one-way authentication like the A1006 using the asymmetric secrets – so it can sign a challenge presented by the host and the host checks then this signature against the public key.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply