Private keys for NXP-provisioned public counterparts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Private keys for NXP-provisioned public counterparts

ソリューションへジャンプ
2,635件の閲覧回数
psvz
Contributor IV

After factory reset of my SE051H I can see quite a few public keys that cannot be removed:

Key-Id: 0X7fff0204   NIST-P            (Public Key)   Size(Bits): 256
Key-Id: 0X7fff020b   NIST-P            (Public Key)   Size(Bits): No Info available
Key-Id: 0X7fff0210   NIST-P            (Public Key)   Size(Bits): 256
Key-Id: 0X7fff0211   NIST-P            (Public Key)   Size(Bits): 256

Particularly, I am curious about "0x7FFF0204 EC Key Used for applet personalization" that seems to allow the private component's holder to ruin the chip effectively. So, who has that private component? Can I get it? Can I disable personalization? 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,583件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Those keys are trust provisioned by NXP , and they are not affected by the deleteall command. 0x7FFF0204 is Applet Feature Management Key, which is created and owned by NXP. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,584件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Those keys are trust provisioned by NXP , and they are not affected by the deleteall command. 0x7FFF0204 is Applet Feature Management Key, which is created and owned by NXP. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信