On A1006 do I have to connect pin 2 (NC) to gnd ? it's said so on A1007 ... Thanks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

On A1006 do I have to connect pin 2 (NC) to gnd ? it's said so on A1007 ... Thanks

1,572 次查看
hassanakhzam
Contributor I

I need a confirmation about pin 2 on A1006 : do I have to connect it to GND like on A1007 ?

Best Regards.

0 项奖励
回复
2 回复数

1,447 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please connect it to ground. For more information please refer to chapter 8.2 Pin description of the data-sheet available under request in DocStore.

Regards,

Ivan.

0 项奖励
回复

1,286 次查看
haryanl
Contributor IV

Hi Ivan

I also have the same question
whether to float pin 2 (N.C) will damage the IC?
Unfortunately in our boards, some of the Security ICs are not working, is the N.C pin the cause?
but when I replace a new IC, it works normally
Looking forward to hearing from you

Best Regards,

Haryanl 

0 项奖励
回复