NFC not clonable and auth from smartphone

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC not clonable and auth from smartphone

2,453 次查看
marta
Contributor I

Hi everyone!

I need to select a NFC tag for user identification in a closed-loop system payment. I have been looking the encryption of different tags such as MIFARE Ultralight C, NTAG 413 DNA or DESFire EV1, but I am not sure which is the most secure. Which is the best option to avoid cloning? 

The tag reader will be an smartphone, all these encryption protocols (3DES, CRYPTO1, AES...) can be used for authentification using an Android or iOS as a reader?

Thanks!

Marta

标签 (1)
0 项奖励
回复
1 回复

2,326 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Marta,

I would recommend Mifare Desfire EV2, which is CC EAL5+ certified. Please refer to MIFARE DESFire EV2 | NXP  for details. Android and iOS are both ok, but for iOS application please use the latest iOS 13.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复