In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

1,627 Views
jordijofrenxp
NXP Employee
NXP Employee

The ISO/IEC 14443 interface of the EdgeLock SE050 gives you the capability to communicate with any NFC phone or contactless reader. Key applications include systems that require late stage product customization, including zero-power configuration and trust provisioning over a contactless reader.

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies