In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In what type of applications can I use the ISO/IEC14443 interface of the EdgeLock SE050?

1,589件の閲覧回数
jordijofrenxp
NXP Employee
NXP Employee

The ISO/IEC 14443 interface of the EdgeLock SE050 gives you the capability to communicate with any NFC phone or contactless reader. Key applications include systems that require late stage product customization, including zero-power configuration and trust provisioning over a contactless reader.

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)