How can I use SE050 with STM32 , can I get MW library files compatible with STM32?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I use SE050 with STM32 , can I get MW library files compatible with STM32?

3,538 Views
Poonam123
Contributor I

How can I use SE050 with STM32 , can I get MW library files compatible with STM32? In MW the supported files are compatible for NXP controllers

0 Kudos
Reply
5 Replies

2,037 Views
Alon1
Contributor I

Hi,

did you succeed?

any code examples will be appreciated. 

0 Kudos
Reply

2,796 Views
Spri
Contributor I

 Hi @Poonam123 , I have similar task to interface the se050 with stm32, are you able to mange porting of mw?

Can you help me in it?

Thanks,

Priyank.

0 Kudos
Reply

3,533 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Poonam123 ,

 

So far the MW just supports NXP MCUs, but we also provide a porting guide for your case. Please kindly refer to https://www.nxp.com/docs/en/application-note/AN12448.pdf for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,524 Views
Poonam123
Contributor I

Hi , Is it possible to operate se050 with simple I2C by configuring apdu? I want to use SE050 without use of library .

 

Thanks

0 Kudos
Reply

3,518 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Poonam123 ,

 

If you just use several commands to communicate with SE050, I would recommend you configure the APDU commands with the help of MW, please kindly refer to "simw-top/doc/demos/se05x/se05x_GetAPDUBuffer/Readme.html" for details.

 

If you are just concerning with the memory consumption of the MW, we provide a tiny version of package instead, please kindly refer to https://github.com/NXPPlugNTrust/nano-package for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply