Generate RSA fails, ssscli

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generate RSA fails, ssscli

ソリューションへジャンプ
2,792件の閲覧回数
psvz
Contributor IV

SE050-E

root@raspberrypi:~ # ssscli generate rsa abc 4096
Generating RSA Key Pair at KeyID = 0x00000ABC,  bits=4096
sss   :INFO :atr (Len=35)
      01 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 00
      01 00 00 00    00 64 13 88    0A 00 65 53    45 30 35 31
      00 00 00
ERROR:sss.keystore:sss_key_store_generate_key FAILED
ERROR! Could not generate RSA Key Pair at KeyID 0x00000ABC

any idea?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,774件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

No, I mean the RSA algorithms are not supported on SE050-E. You may generate an ECC Key pair instead for encrypt/decrypt purpose.

Kan_Li_0-1672195900379.pngKan_Li_0-1672195900379.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,783件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

RSA is not supported on SE050-E, please use SE051/SE050F instead for that purpose.

 

Sorry for the confusion that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,779件の閲覧回数
psvz
Contributor IV

@Kan_Li is it only for "generate" that isn't supported - can I inject my own RSA 4096 bits key? Besides, is there any EC-type key that SE050 can use to decrypt a message e.g., 25519 curve can be used for encrypt/decrypt (check Secret Key Encryption — PyNaCl 1.6.0.dev1 documentation) but you could use other EC keys for that...

0 件の賞賛
返信
2,775件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

No, I mean the RSA algorithms are not supported on SE050-E. You may generate an ECC Key pair instead for encrypt/decrypt purpose.

Kan_Li_0-1672195900379.pngKan_Li_0-1672195900379.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信