Failure in Se05x_API_SessionOpen on SE052F (Raspberry Pi I2C Communication Issue)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure in Se05x_API_SessionOpen on SE052F (Raspberry Pi I2C Communication Issue)

11,339 Views
krsuresh
Contributor III

Hi Team,

I am facing an issue while trying to communicate with the SE052F over I2C using the Plug & Trust Nano Package.
According to the AN14277 application note, I configured the SCP03 keys as follows:

ENC Key: 3ae441c747e32ebc16b3bb2d843c6dd8
MAC Key: 6c18f3d08fee1cb96a3c8de5d3538aaa

However, Se05x_API_SessionOpen consistently fails.

System Information
Platform: Raspberry Pi
Package: Plug and Trust Nano Package v1.5.4
Example used: ex_se05x_GetInfo

 

Log Details:

./ex_se05x_GetInfo
Se05x Getinfo Example !
Plug and Trust nano package - version: 1.5.4
I2C driver supports plain i2c-level commands.
APDU Tx> :00 a4 04 00 0b d2 76 00 00 85 30 4a 43 4f 90 03 00
Failed writing data (nrWritten=-1).
Se05x_API_SessionOpen failedError in Se05x_API_SessionOpen
SE05x Getinfo Example Failed !

I2C Detect details in Raspberry Pi:
flexxon@raspberrypi:~/SE050/NEW-NANO/se052f/nano-package/examples/se05x_GetInfo/linux/build $ i2cdetect -y 1
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- 48 -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

 

Thanks,

Sureshkumar R

Labels (1)
0 Kudos
Reply
23 Replies

10,663 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

Since you are testing this on Raspberry Pi , did you also test with the full version of MW? Did it work anyway? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

10,660 Views
krsuresh
Contributor III

Hi @Kan_Li,

 

Thanks for the quick response.

I used the following configuration during the simw_top build, and while se05x_GetInfo runs successfully, se05x_Minimal fails; the log is provided below.

PTMW_ Applet = SE05X_C
PTMW_ FIPS = None
PTMW_ SE05X_ Ver = 03_XX
PTMW_SE05X_Auth = PlatfSCP03
PTMW_ SCP = SCP03_SSS
SSSFTR_ SE05X_ RSA = disable/enable

./se05x_GetInfo
Failed to export Enable pin : Invalid argument
Failed to open GPIO value file : No such file or directory
Failed to unexport GPIO : Invalid argument
App :INFO :Running ./se05x_GetInfo
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :PlugAndTrust_v04.07.01_20250519
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
App :WARN :#####################################################
App :INFO :uid (Len=18)
04 00 50 01 39 97 7A C3 BF 57 52 04 26 1F 32 0A
1D 90
App :INFO :Running ./se05x_GetInfo
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
sss :INFO :Newer version of Applet Found
sss :INFO :Compiled for 0x70200. Got newer 0x70216
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
App :WARN :#####################################################
App :INFO :Applet Major = 7
App :INFO :Applet Minor = 2
App :INFO :Applet patch = 22
App :INFO :AppletConfig = 26F2
App :INFO :With ECDSA_ECDH_ECDHE
App :INFO :WithOut EDDSA
App :INFO :WithOut DH_MONT
App :INFO :With HMAC
App :INFO :With RSA_PLAIN
App :INFO :With RSA_CRT
App :INFO :With AES
App :INFO :WithOut DES
App :INFO :With PBKDF
App :INFO :With TLS
App :INFO :WithOut MIFARE
App :INFO :With I2CM
App :INFO :Internal = FFFF
App :WARN :#####################################################
App :INFO :Tag value - proprietary data 0xFE = 0xFE
App :INFO :Length of following data 0x45 = 0x4F
App :INFO :Tag card identification data (Len=2)
DF 28
App :INFO :Length of card identification data = 0x4C
App :INFO :Tag configuration ID (Must be 0x01) = 0x01
App :INFO :Configuration ID (Len=12)
00 05 B5 01 1B 7D B8 1B 89 99 D0 5D
App :INFO :OEF ID (Len=2)
B5 01
App :INFO :Tag patch ID (Must be 0x02) = 0x02
App :INFO :Patch ID (Len=8)
00 00 00 00 00 00 00 00
App :INFO :Tag platform build ID1 (Must be 0x03) = 0x03
App :INFO :Platform build ID (Len=24)
4A 33 52 36 30 30 30 33 37 33 31 38 31 32 30 30
6D 20 B6 19 7D 63 5E 7C
App :INFO :JCOP Platform ID = J3R6000373181200
App :INFO :Tag FIPS mode (Must be 0x05) = 0x05
App :INFO :FIPS mode var = 0x01
App :INFO :Tag pre-perso state (Must be 0x07) = 0x07
App :INFO :Bit mask of pre-perso state var = 0x00
App :INFO :Tag ROM ID (Must be 0x08) = 0x08
App :INFO :ROM ID (Len=8)
B3 37 5F E9 B5 50 8B C4
App :INFO :Tag JCOP OS Core ID (Must be 0x0A) = 0x0A
App :INFO :JCOP OS Core (Len=8)
55 60 6F D4 BE EC F3 CD
App :INFO :Status Word (SW) (Len=2)
90 00
App :INFO :se05x_GetInfoPlainApplet Example Success !!!...
App :WARN :#####################################################
App :INFO :cplc_data.IC_fabricator (Len=2)
47 90
App :INFO :cplc_data.IC_type1 (Len=2)
D6 00
App :INFO :cplc_data.Operating_system_identifier (Len=2)
47 00
App :INFO :cplc_data.Operating_system_release_date (Len=2)
00 00
App :INFO :cplc_data.Operating_system_release_level (Len=2)
00 00
App :INFO :cplc_data.IC_fabrication_date (Len=2)
41 02
App :INFO :cplc_data.IC_Serial_number (Len=4)
38 51 87 21
App :INFO :cplc_data.IC_Batch_identifier (Len=2)
02 67
App :INFO :cplc_data.IC_module_fabricator (Len=2)
00 00
App :INFO :cplc_data.IC_module_packaging_date (Len=2)
00 00
App :INFO :cplc_data.ICC_manufacturer (Len=2)
00 00
App :INFO :cplc_data.IC_embedding_date (Len=2)
00 00
App :INFO :cplc_data.IC_OS_initializer (Len=2)
19 26
App :INFO :cplc_data.IC_OS_initialization_date (Len=2)
1F 38
App :INFO :cplc_data.IC_OS_initialization_equipment (Len=4)
35 31 38 37
App :INFO :cplc_data.IC_personalizer (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_date (Len=2)
00 00
App :INFO :cplc_data.IC_personalization_equipment_ID (Len=4)
00 00 00 00
App :INFO :cplc_data.SW (Len=2)
90 00
App :INFO :ex_sss Finished
Failed to open GPIO value file : No such file or directory
Failed to unexport GPIO : Invalid argument
Failed to unexport GPIO : Invalid argument

 

flexxon@raspberrypi:~/SD/simw-top_build/raspbian_native_se050_t1oi2c/bin $ ./se05x_Minimal
Failed to export Enable pin : Invalid argument
Failed to open GPIO value file : No such file or directory
Failed to unexport GPIO : Invalid argument
App :INFO :Running ./se05x_Minimal
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :PlugAndTrust_v04.07.01_20250519
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
sss :INFO :Newer version of Applet Found
sss :INFO :Compiled for 0x70200. Got newer 0x70216
sss :WARN :Communication channel is Plain.
sss :WARN :!!!Not recommended for production use.!!!
sss :WARN :nxEnsure:'ret == SM_OK' failed. At Line:7839 Function:sss_se05x_TXn
sss :WARN :APDU Transaction Error: Conditions not satisfied (0x6985)

App :ERROR:Se05x_API_GetFreeMemory Failed
App :INFO :mem=0
App :ERROR:se05x_Minimal Example Failed !!!...
App :INFO :ex_sss Finished
App :ERROR:ex_sss_entry Failed
App :ERROR:!ERROR! ret != 0.

 

Thanks,

Sureshkumar R

0 Kudos
Reply

10,623 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

Did you really rebuild the MW with the following options?

PTMW_ SE05X_ Ver = 03_XX
PTMW_SE05X_Auth = PlatfSCP03

From the log, there are some conflicts:

sss :INFO :Compiled for 0x70200. Got newer 0x70216
sss :WARN :Communication channel is Plain.

 

Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

10,612 Views
krsuresh
Contributor III

Hi @Kan_Li,

Please find the test result log below. Let me know if you need any additional information for further analysis.


flexxon@raspberrypi:~/SD/simw-top_build/raspbian_native_se050_t1oi2c/bin $ ./se05x_GetInfo
Failed to export Enable pin : Invalid argument
Failed to open GPIO value file : No such file or directory
Failed to unexport GPIO : Invalid argument
App :INFO :Running ./se05x_GetInfo
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :PlugAndTrust_v04.07.01_20250519
App :INFO :Using default PlatfSCP03 keys. You can use keys from file using ENV=EX_SSS_BOOT_SCP03_PATH
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
scp :WARN :nxEnsure:'status == kStatus_SSS_Success' failed. At Line:148 Function:nxScp03_AuthenticateChannel
sss :ERROR:Could not set SCP03 Secure Channel
App :ERROR:sss_session_open failed
App :ERROR:ex_sss_session_open Failed
App :ERROR:!ERROR! ret != 0.

 

flexxon@raspberrypi:~/SD/simw-top_build/raspbian_native_se050_t1oi2c/bin $ ./se05x_Minimal
Failed to export Enable pin : Invalid argument
Failed to open GPIO value file : No such file or directory
Failed to unexport GPIO : Invalid argument
App :INFO :Running ./se05x_Minimal
App :INFO :If you want to over-ride the selection, use ENV=EX_SSS_BOOT_SSS_PORT or pass in command line arguments.
App :INFO :PlugAndTrust_v04.07.01_20250519
App :INFO :Using default PlatfSCP03 keys. You can use keys from file using ENV=EX_SSS_BOOT_SCP03_PATH
sss :INFO :atr (Len=35)
01 A0 00 00 03 96 04 03 E8 00 FE 02 0B 03 E8 00
01 00 00 00 00 64 13 88 0A 00 65 53 45 30 35 31
00 00 00
sss :INFO :Newer version of Applet Found
sss :INFO :Compiled for 0x30100. Got newer 0x70216
scp :WARN :nxEnsure:'status == kStatus_SSS_Success' failed. At Line:148 Function:nxScp03_AuthenticateChannel
sss :ERROR:Could not set SCP03 Secure Channel
App :ERROR:sss_session_open failed
App :ERROR:ex_sss_session_open Failed
App :ERROR:!ERROR! ret != 0.

 

krsuresh_0-1764819353609.png

 

Thanks,

Sureshkumar R

0 Kudos
Reply

10,606 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

Thanks for the info! Seems the platformSCP keys used in your test are not for SE052F, would you please configure the keys according to the guide in SE-PLUG-TRUST-MW_04.07.01/simw-top/doc/appendix/platfscp.html? 

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

10,589 Views
krsuresh
Contributor III

Hi @Kan_Li,

Thanks for the update. Yes, the MW is working fine now after configuring the correct PlatformSCP keys. However, I noticed something unusual: the Plug & Trust Nano package samples are also working now without any code changes, even though they were failing earlier. I’m not able to understand how they started working suddenly. Could you please help clarify what might cause this behavior?

 

flexxon@raspberrypi:~/SE050/NEW-NANO/se052f/nano-package/examples/se05x_crypto/linux/build $ ./ex_se05x_crypto
Se05x crypto Example !
Plug and Trust nano package - version: 1.5.4
I2C driver supports plain i2c-level commands.
Establish Secure Channel to SE05x !
Created scp03 Session
Get Version ==>
Applet Version 7.2.22
ex_get_version, PASSED
ex_generate_nist256_key, PASSED
ex_set_get_nist256_key, PASSED
ex_nist256_sign_verify, PASSED
ex_generate_nist384_key, PASSED
ex_set_get_nist384_key, PASSED
ex_nist384_sign_verify, PASSED
ex_set_certificate, PASSED
ex_ecdh, PASSED
ex_aes_ECB_NOPAD, PASSED
ex_aes_CBC_NOPAD, PASSED
ex_aes_CTR, PASSED
ex_nist256_sign_policy, PASSED
ex_read_attst_object, PASSED
Close i2c device 3.
SE05x crypto Example Success !

 

Thanks,

Sureshkumar R

0 Kudos
Reply

10,495 Views
krsuresh
Contributor III

Hi @Kan_Li,

 

I am testing two new SE052F boards. On the first board, the Plug & Play Nano package sample initially failed, but after running the Middleware sample once with plain_scp.txt, both Middleware and Nano samples started working correctly.

However, when I switch to the second new board and test the Nano package, it fails. After that, when I switch back to the first board, the Nano package also fails again. It seems that running the Middleware sample with plain_scp.txt is required each time to make the Nano package work.

Could you please help clarify why the Plug & Play Nano sample behaves inconsistently when switching between different SE052F boards? Is there any configuration or reinitialization needed for each board before running the Nano package?

 

Thanks,

Sureshkumar R

0 Kudos
Reply

10,488 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

How did you connect SE05x with the raspberry board? If you connect them via wires, maybe you can connect the RST pin to VCC directly to avoid the SE hold in reset. 

Kan_Li_0-1764910314471.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply

10,460 Views
krsuresh
Contributor III

Hi @Kan_Li,

I have tested the setup by connecting the RST pin to VCC as suggested, but the issue still persists. Additionally, I have observed that when I run the Middleware sample first, both the Middleware and the Nano package function correctly. However, after disconnecting and reconnecting the power to the SE052F board, the Nano package fails to work again.

Thanks,

Sureshkumar R

0 Kudos
Reply

9,881 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

I can reproduce this issue here and checking with the MW team now, will let you know when there is any progress,

 

Thanks for your patience!

 

Best Regards,

Kan

0 Kudos
Reply

9,100 Views
krsuresh
Contributor III

Hi @Kan_Li 

Thank you for the update.

Just checking if there is any progress or update from the MW team on this issue.
Please let me know when you have any information.

Thanks,
Sureshkumar R

0 Kudos
Reply

9,066 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

I am sorry, but so far there is no response from the MW team due to the holidays, while as a quick solution, you may use a longer timer interval as below:

Kan_Li_0-1766990511717.png

The source file can be found in nano-package-master/lib/platform/linux/ .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

7,967 Views
krsuresh
Contributor III

Hi @Kan_Li,

As suggested, I increased the timer interval, but I am still facing the same behavior.
Is there any update from the MW team on this issue?

 

Thanks,

Sureshkumar R

0 Kudos
Reply

7,211 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @krsuresh ,

 

Have you tried a larger value instead? The MW has put this in plan, but the fix I would expect to be the next release.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

6,769 Views
Ben-FLX
Contributor I

@Kan_Li Do you know of any scheduled release that happens on regular interval in which we can expect this to be made available?

For e.g, within every quarter, or every Q1 & Q3?

If it is not something that is happening soon, then we need to know whether there is any possibility for a off-cycle release such that it does not affect our development activity.

 

Otherwise, we may have to consider other options such as going back to using SE050 (for our upcoming prototype build) and understand what it takes to migrate to SE052.

0 Kudos
Reply

6,730 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Ben-FLX ,

 

We could plan for a release on the end of Feb 2026 along with our Main Package Release. Does it align with your timeline?

 

Best Regards,

Kan

0 Kudos
Reply

6,721 Views
Ben-FLX
Contributor I

Hi @Kan_Li 

Yes, end feb works as long as we are able to execute all supported code/functions supplied by the package using SE052 eval board. Of course, the earlier this package can be made available, the better it is for us.

Lastly, what is a good way for us to be notified when the new package becomes available? I am not sure why I am not receiving email notifications here and I don't see myself refreshing NXP website on a daily basis to check for updates.

0 Kudos
Reply

6,719 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Ben-FLX ,

 

Thanks for the clarification! I will let the MW team know about this. and for notification, I think you may use the notify function from the github, as shown below:

Kan_Li_0-1769759900876.png

 

and anyway, you may reach out to me here at anytime.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

6,411 Views
Ben-FLX
Contributor I

@Kan_Li Just wondering, any update/news about the planned code release? Is it progressing smoothly?

0 Kudos
Reply

6,353 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Ben-FLX ,

 

I just checked with the MW team, the fix would be available by Mar 31st. Due to other priorities this is delayed. Sorry for the inconvenience that has caused.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply