Error messages with se5x when reading id list

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error messages with se5x when reading id list

880 Views
Jamier
Contributor III

I am working with a provisioned secure element se050 and I am suddenly getting error messages instead of the id list.

I use these commands and I would normally get an output of a bunch of key ids.

ssscli connect se05x t1oi2c non

ssscli se05x readidlist

 

But suddenly I am seeing these two error messages on two different chips:

ERROR:cli.cli:invalid load key, '\x00'.
ERROR:cli.cli:'Context' object has no attribute 'session'

ERROR:cli.cli:Ran out of input
ERROR:cli.cli:'Context' object has no attribute 'session'

A power cycle doesn't help.

Does anyone know what's going on? 

The devices these chips have been installed on have been undergoing stress and environmental testing -40C to +65C. 

 

Thanks.

 

 

 

Labels (1)
0 Kudos
Reply
2 Replies

844 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Jamier ,

 

Which variant of SE05x was used in your test? Have you tried to rebuild sssapisw within the MW with the verbose log level? It would be very helpful to have the log during this issue.

Kan_Li_0-1728886754904.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply

736 Views
Jamier
Contributor III

Thanks for the suggestion.

I ended up getting it working by reprogramming my BSP. I didn't try the verbose log as I didn't have the time to do the setup for that. I suspect the problem was caused by corrupted files and not by anything to do with the chip or the i2c communication.

0 Kudos
Reply