Does the EdgeLock SE050 applet support sensor data protection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the EdgeLock SE050 applet support sensor data protection?

2,098件の閲覧回数
jordijofrenxp
NXP Employee
NXP Employee

Yes, it does. The EdgeLock SE050 allows you to set up a secure, end-to-end connection from the
sensor or actuator to your local IoT gateway or cloud-based service, protecting the
interface between the sensor and the security IC. As such, EdgeLock SE050 helps you to
provide a higher level of security in your IoT system by:

  • Preventing data manipulation: The data extracted by the sensor is collected privately
    and cannot be manipulated.
  • Authenticating the sensor: The system authenticates the sensor as a proof of origin.
  • Providing end-to-end security: The data collected over the private sensor can be
    encrypted and securely transferred to your gateway or cloud for further treatment and
    analysis.

For more information, you can refer to AN12449- Sensor data protection with EdgeLock SE050

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)