Does the EdgeLock SE050 Plug & Trust middleware support non NXP MCU / MPU boards?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the EdgeLock SE050 Plug & Trust middleware support non NXP MCU / MPU boards?

3,557 Views
jordijofrenxp
NXP Employee
NXP Employee

The EdgeLock SE050 Plug & Trust middleware comes with pre-built support for many NXP MCU / MPU boards. However, you can also leverage SE050 Plug & Trust middleware if you are using any other MCU / MPU board.

From an HW perspective, you can use the OM-SE050ARD evaluation board to connect your board via the Arduino connectors or the external I2C connector.

From an SW perspective, The EdgeLock SE050 Plug & Trust middleware has been designed to facilitate portability to multiple platforms and OS. For more information about how to port the middleware, you can refer to AN12448 SE050 Plug & Trust middleware porting guidelines.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,569 Views
rodolfoveltrigo
NXP Employee
NXP Employee

Hi all,

this is the new NXP weblink of this application note (old link does not work anymore).

https://www.nxp.com/docs/en/application-note/AN12448.pdf

Cheers

Rodolfo

0 Kudos
Reply