Copying a NTAG 424 DNA without opening the URI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Copying a NTAG 424 DNA without opening the URI

3,821件の閲覧回数
gabriele
Contributor I

Hi,

I'm interested in NTAG424 DNA. 

I understand that the SUN message is based on URL, UID, and counter, so that the generated string is different each time is read. I guess that the server keep trace of each UIDs' counter.

But what if I copy the string of a DNA tag (without actually opening the link), and paste on a new tag?

That string should still be valid, since the server doesn't know it's been read. The copied link would be valid (just the 1st time is read). Is that correct? 

Thank you.

ntag424 #ntag413‌ #ntag 413 dna‌ #cmac‌

2 返答(返信)

3,722件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, the server would accept it given the original NTAG 424 DNA was not read again before that time, otherwise the server would detect it.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,722件の閲覧回数
gabriele
Contributor I

Thank you, Kan.

Have a great day!

0 件の賞賛
返信